Manufacturing in US and Singapore
Stock and Custom, from Design and Prototype to Volume Production
MRF Fine Finishing Consistently Exceeding λ/40 Surface Accuracy
Contact UsEdmund Optics® manufacturers millions of optics every year throughout our four global facilities. Join us as we take you through the creation of an aspheric lens, from molding to grinding to polishing, centering, and metrology.
Aspheric Lenses, also known as Aspherical Lenses, are used to eliminate spherical aberration in a range of applications, including barcode scanners, laser diode collimation, or OEM or R&D integration. Aspheric lenses utilize a single element design which helps minimize the number of lenses found in multi-lens optical assemblies. Said another way, unlike conventional lenses with a spherical front surface, aspheric lenses have a more complex front surface that gradually changes in curvature from the center of the lens out of the edge of the lens. This reduction in total element count not only helps decrease system size or weight, but also simplifies the assembly process. Integrating aspheres into an application such as focusing the output of a laser diode may not only decrease total cost, but may also outperform assemblies designed with traditional spherical optical lenses.