Edmund Optics uses cookies to optimize and enhance the features and content on our website. Click “OK” for the full user experience, you can view additional information on the cookies we use by clicking the “Details” button. We do NOT sell your information from marketing cookies, we use it to improve ONLY YOUR experience with Edmund Optics.
Some of the data collected by this provider is for the purposes of personalization and measuring advertising effectiveness.
Some of the data collected by this provider is for the purposes of personalization and measuring advertising effectiveness.
Some of the data collected by this provider is for the purposes of personalization and measuring advertising effectiveness.
Some of the data collected by this provider is for the purposes of personalization and measuring advertising effectiveness.
Cookies are small text files that can be used by websites to make a user's experience more efficient.
The law states that we can store cookies on your device if they are strictly necessary for the operation of this site. For all other types of cookies we need your permission.
This site uses different types of cookies. Some cookies are placed by third party services that appear on our pages.
You can at any time change or withdraw your consent from the Cookie Declaration on our website.
Learn more about who we are, how you can contact us and how we process personal data in our Privacy Policy.
Please state your consent ID and date when you contact us regarding your consent.
Most web browsers allow you to view your cookies in the browser preferences, typically within the "Privacy" or "Security" tab. Some browsers allow you to delete specific cookies or even prevent cookies from being created. While disallowing cookies in your browser may provide a higher level of privacy, it is not recommended since many websites require cookies to function properly. Alternatively, you can visit www.aboutcookies.org which provides directions on how to block or delete cookies on all major browsers.
|
Captures images of objects around corners and behind obstacles |
|
Light scattered back off of hidden target used to reconstruct a 3D model of the target |
|
Involves scattering laser light off of surrounding objects onto a hidden target |
|
Many potential benefits for autonomous vehicles, public health, and medical imaging |
A direct line of sight between an object and a camera or detector is typically needed for every imaging application except for extreme cases such as light bending due to gravitational lensing in astronomy. But for the most part, imaging applications are limited to light propagating in a straight line. However, that is starting to change as some cutting edge research is opening up possibilities to image around corners and around obstacles. A combination of lasers, sensitive cameras, and computational reconstruction methods can be used to detect objects hidden by obstacles by scattering light off of surrounding objects.
The process for non-line-of-sight imaging is similar to that of LiDAR (light detection and ranging), where a laser pulse is sent towards an object and the time-of-flight of the light scattering back off of the object is used to measure the distance between the object and a detector. However, non-line-of-sight imaging images objects obscured by obstacles by adding another scattering event to this process.1
Highly sensitive cameras such as single-photon avalanche photodiode array cameras are needed to measure the propagation of picosecond and femtosecond pulses of light in real time. The detector receives two different return signals: an initial signal of light scattered directly off of the wall and a secondary signal of light scattered off of the target, which is the signal used for non-line-of-sight imaging. This time-of-flight information is then used to reconstruct a series of ellipsoids that all overlap at a given point on the hidden target, allowing computational software to calculate the distance between the camera and the hidden target and recreate a 3D model of the target.
A 3D object can be broken down into a collection of many individual points that scatter light. The summation of all of these points can reconstruct a model of the original object. If the detector can distinguish return pulses with a temporal resolution of 100ps, this corresponds to a spatial resolution of points on the hidden target of approximately 1.5cm. 1
Allow cars to sense approaching vehicles or pedestrians around corners before they are in the car’s direct line of sight2
Let law enforcement, firefighters, and emergency medical services detect presence of people in dangerous situations from a safe distance2
Investigate small 3D structures hidden from the system’s direct line of sight2
Taking this emerging technology and creating a practical solution for real-world use that is portable and not dangerous to observer’s eyes is extremely challenging. One of the main issues with non-line-of-sight imaging is the limited amount of light that makes its way back to the detector, which must be able to pick up this very small amount of light and differentiate it for any ambient light sources. The return signal to the detector is the result of two consecutive scattering events, leading to an extremely high loss. Return signals can be as low as one photon per laser pulse.1
However, the Stanford Computational Imaging Lab has developed a non-line-of-sight imaging system that works outdoors under indirect sunlight.2 They successfully imaged an object made out of retroreflective tape that was obscured by a wall, which bodes well for the future of this technology.
The lab of Aristide Dogariu of University of Central Florida is investigating non-line-of-sight imaging utilizing the spatial coherence of light hitting a wall instead of laser light scattered off of that wall and the target behind it.3 This could lead to modeling of the hidden target without requiring ultrafast laser illumination, making real-world applications of the technology more portable and easy to use.
More development is still needed before non-line-of-sight imaging technology becomes available in practical commercial systems, but it is a promising solution for the next generation of imaging applications.
Edmund Optics® (EO) designs and manufactures imaging lenses and ultrafast laser optics, which are both used in non-line-of-sight imaging systems.
The light scattering directly off of the wall is much stronger than the secondary scatter of light off of the indirect object, but there is a time delay between them that allows highly sensitive detectors with a high enough temporal resolution to differentiate the two signals.2
The software first stores all measurements in a 3D spatial-temporal volume. It then resamples measurements along the time axis, convolves the result with an inverse filter in the frequency domain, and resampling result along depth axis to recover the hidden object.2
The Stanford Computational Imaging Lab’s non-line-of-sight imaging procedure only takes 0.5s to generate the 3D model.2