Fluorescent illumination is based off of using electrodes inside of glass tubes to first ionize an inert gas, which in turn excites electrons in Mercury atoms. These excited electrons then release photons that excite a phosphor coating on the inside of the glass tube, which is ultimately responsible for the wavelengths of light put out by the particular fluorescent bulb.
Cool, compact, and economical, Fluorescent Illumination provides flicker-free lighting with consistent color temperature. White bulbs, specific color bulbs, and black (UV) bulbs are readily interchangeable for different applications. Long lifetimes and low profiles make fluorescent illumination a great choice for industrial as well as microscopy applications. Optional black bulbs are very useful for UV inspection and UV curing applications.
1-800-363-1992
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2025 | Edmund Optics, Ltd Unit 1, Opus Avenue, Nether Poppleton, York, YO26 6BL, UK
California Consumer Privacy Acts (CCPA): Do Not Sell or Share My Personal Information
California Transparency in Supply Chains Act