eo_logo
 
Product added to cart
All Press Releases

Edmund Optics® Offers Diamond Turning Technique

Process Produces High Precision Optical Components

7/17/2018, Barrington, NJ USA   —

Edmund Optics® (EO), the premier provider of optical components, utilizes single point diamond turning to produce a wide range of high precision optical components. The manufacturing technique involves mechanical machining of precision elements using lathes or other machines equipped with diamond-tipped tool bits. This ultra-precise machining process generates desired surface profiles with accuracies of a few nanometers or less.

Precision optical components produced from metals, plastics, and crystalline materials

Edmund Optics uses single point diamond turning to produce off-axis parabolic (OAP) mirrors, off-axis elliptical (OAE) mirrors, and other precision metal, plastic, and crystalline optical components. Off-axis focusing mirrors are free of aberrations across a broadband range, which is ideal for use in instrumentation and laser systems. Edmund Optics’ diamond turning capabilities are available in three grades: Commercial (λ wavefront error and 80-50 surface quality), Precision (λ/2 wavefront error and 60-40 surface quality), and High Precision (λ/8 wavefront error and 40-20 surface quality). Edmund Optics can also achieve RMS surface roughness values as low as 30Å. A variety of coatings are available, including uncoated, aluminum, protected gold, bare gold, and custom coatings.

Diamond turning video demonstration

Edmund Optics released a video showing footage of optical components being diamond turned. The video demonstrates the strict environmental controls on temperature, cleanliness, and vibration required for diamond turning.

Process improvement reduces setup time, increases lot sizes, and minimizes waste

The video also outlines the data collection process during inspection – monitoring surface quality, surface roughness and mechanical inspection. Process improvement is a priority for Edmund Optics, including Six Sigma, LEAN processes, and Kaizen events, resulting in reduced setup time, increased lot sizes, and minimized waste. An in-house machine shop allows for streamlined creation of tooling and blanks, further reducing lead times.

Metrology instruments inspect and ensure highest quality

A variety of metrology instruments inspect the diamond turned parts to ensure the highest quality including interferometers, profilometers, and coordinate measuring machines. In addition to the large selection of standard optical components,Edmund Opticsoffers build-to-print or custom capabilities to meet exact customer specifications. Edmund Optics’s diamond turning staff has extensive experience in optimizing designs for manufacturability and cost reduction.

About Edmund Optics:

Edmund Optics® is a leading supplier of optics, imaging, and photonics technology for the Life Sciences, Biomedical, Semiconductor, R&D, and Defense markets around the globe.Edmund Opticsdesigns and manufactures a wide array of multi-element lenses, lens coatings, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of both stock and custom products. Edmud Optics’ state-of-the-art manufacturing capabilities, combined with its global distribution network, has earned it the position of the world’s largest supplier of off-the-shelf optical components. Customers can purchase items by calling 1-800-363-1992, via the catalog or the website at www.edmundoptics.com.