eo_logo
 
Product added to cart
Edmund Optics® does not sell the VERI-Q PCR 316. Inquiries about the device itself should be directed to MiCo BioMed.
ITOS Trutzschler

Case Study:
Diagnosing the Novel Coronavirus with Optics

The future depends on rapidly detecting and treating contagious diseases, such as COVID-19, which is caused by the novel coronavirus.

Quick, Reliable, and Accurate
COVID-19 Testing

The COVID-19, which is caused by the novel coronavirus, pandemic has brought about a global health crisis. Now more than ever, quick, reliable, and accurate testing is critical for reducing the impact of this infectious disease. South Korean healthcare diagnostics company, MiCo BioMed, has developed a rapid, highly-sensitive molecular diagnostic device called the VERI-Q PCR 316 that can detect COVID-19 within one hour.

This portable device utilizes optical filters, beamsplitters, lenses, and mirrors in a real-time reverse transcription polymerase chain reaction (rRT-PCR) test, in which a small sample of DNA is amplified and studied in detail. Producing test results in less than one hour makes the VERI-Q PCR 316 a powerful tool for fighting the spread of COVID-19. The VERI-Q PCR 316 is currently being used across the globe in countries including Poland, Hungary, Romania, Ecuador, Bangladesh, Senegal and Brazil.  

 Trützschler developed the T-SCAN Camera (4-CCD), which makes observations from 4 different canals while utilizing ITOS polarization filters at key positions to make contaminants detectable

Genetic material from nasal swabs is added to a unique test solution. Sample DNA is exponentially replicated during the rRT-PCR test to allow for accurate analysis.

The US Centers for Disease Control (CDC) has approved RT-PCR tests for combatting the spread of COVID-19.1
Quick, Reliable, and Accurate COVID-19 Testing

Speed is Critical for Tackling Global Health Challenges

Other diagnostic tests for COVID-19 may exceed 24 hours to produce results, making them impractical for testing at airports and borders. The VERI-Q PCR 316 utilizes real time PCR screening to analyze patients within one hour, meaning travellers may wait at the sample collection point for their test results. If the test comes back negative, the patient can be released; if the test is positive, they can be isolated and treated.  

How Are Optics Used in COVID-19 Detection?

Many PCR screening systems rely on fluorescence, where targeted double-stranded DNA molecules are tagged with fluorescent dyes that emit light when exposed to a shorter wavelength input.2 These devices follow a similar schematic to fluorescence microscopes (Figure 1).

SpectralMD’s wound imaging system in use
Figure 1: The optical design of fluorescence-based PCR screening systems like VERI-Q PCR 316 resembles this setup of a simple fluorescence microscope.

An excitation filter allows wavelengths from the illumination source that would excite the fluorescent sample to pass. These excitation wavelengths reflect off a dichroic filter and are focused onto the sample by lenses. Fluorescent emission from the sample transmits through the dichroic filter towards lenses that focus the light onto the system’s detectors. Measuring the amount of fluorescence lets the PCR screening system determine the presence of molecules that would indicate if a sample is COVID-19 positive.

Edmund Optics is proud to supply optical components for life-saving applications like MiCo BioMed’s VERI-Q PCR 316. This device, along with countless other optics-enabled technologies, are helping create a safer and healthier future.  

References

  1. "ACCELERATED EMERGENCY USE AUTHORIZATION (EUA) SUMMARY COVID-19 RT-PCR TEST." Laboratory Corporation of America, Mar. 2020.
  2. "Real Time PCR." PREMIER Biosoft, www.premierbiosoft.com/tech_notes/real_time_PCR.html.
Was this content useful to you?
Bandpass Filters TECHSPEC LOGO

Bandpass Filters

  • Bandwidths as Small as 5nm
  • Common Wavelengths for Popular Fluorophores
  • Kits of Multiple Filter Options Available

View Now
Beamsplitters TECHSPEC LOGO

Beamsplitters

  • Plate, Cube, Pellicle, and Other Specialty Types
  • Polarizing, Non-Polarizing, and Laser Line Versions Available
  • Coating Options from 350 – 1620nm
View Now
Optical Lenses TECHSPEC LOGO

Optical Lenses

  • Spherical, Aspheric, and Achromatic Lenses
  • Vast Selection of Sizes and Coatings
  • Glass, Plastic, and Crystalline Lenses for Every Application
View Now
Optical Mirrors TECHSPEC LOGO

Optical Mirrors

  • Wide Range of Metallic and Dielectric Coatings
  • Flat, Focusing, or Specialty Mirrors
  • High Laser-Induced Damage Threshold Versions

View Now
The Future Depends on Optics